rfbee and I2C (BMP085 sensor)

HI,

If I understood correctly If you are using RFBee on XBeeCarrier board then you need to turn on mosfet (drive A2 low)

But in this case I have xBee on the breadboard (raw deployment) connecting directly to BMP085 sensor.
I cannot get this to work (BMP085 works on Arduino Uno Pin4 and Pin5 connected).
Based on my research RFBee Pins PC4 and PC5 are I20 SDA and SCL ports so It should work.
I initiate the communication but when trying to wake up BMP085 sensor I get garbage on serial port (so it looks like something is definitely wrong).

Could it be that firmware need to be initialized or something ?

Thanx,
DiNo