reTerminal with CM5?

Hi there,

So, If I were betting I would think two things from watching these spaces,
the more likely canadate would be the :crossed_fingers: reTerminal DM

reTerminal DM, a 10.1" open-source industrial Human-Machine Interface (HMI) that serves as an Integrated Device Master. This all-in-one device, based on Raspberry Pi CM4, functions as a Panel PC, HMI, PLC, and IIoT Gateway. With an IP65 industrial-grade large screen, reTerminal DM is a next-gen interactive sensing hub, streamlining data flow and onsite device management."
Could be updated maybe… or

Sweet platform maybe… :grin: :+1:

GL :slight_smile: PJ :v: