Yes, it works on JetPack v4.4 Image.
We driver a sensor with spi interface on /dev/spidev0.0
The error report your system lose /dev/spidev0.1
self.spi.open(bus, device) # Open SPI port 0, slave device (CS) 1 FileNotFoundError: [Errno 2] No such file or directory
You need change the code to set argument device to 0.
Then use this device tree overlay.