Regarding 2 spi interface in seeed studio nrf52840

I tried it with my BMP388 instead of the MAX30003. The SD part is a copy of your sketch.Even with the SPI clock set to 32 MHz, both SD and BMP388 operated without problems.
In your sketch, you operate the chip select to LOW and HIGH before and after accessing the device, but I don’t think this is necessary.

I don’t know if this will be helpful, but here is a sketch I tried.

#include <SPI.h>
#include <Adafruit_Sensor.h>
#include <Adafruit_BMP3XX.h>
#include <SD.h>

#define BMP_SCK D8
#define BMP_MISO D9
#define BMP_MOSI D10
#define BMP_CS D7
#define chipSelect D0

#define SEALEVELPRESSURE_HPA (1013.25)

Sd2Card card;
SdVolume volume;
SdFile root;
Adafruit_BMP3XX bmp;

void setup() {
  Serial.begin(115200);
  while (!Serial);
  delay(2000);
  Serial.println("BMP388 / SD SPI TEST");

  // SD card Initialization
  Serial.print("\nInitializing SD card...");
  pinMode(chipSelect,OUTPUT);
  digitalWrite(chipSelect,LOW); //enable device
//  if (!card.init(SPI_HALF_SPEED, chipSelect)) {
  if (!card.init(32000000UL, chipSelect)) {    
    Serial.println("initialization failed. Things to check:");
    Serial.println("* is a card inserted?");
    Serial.println("* is your wiring correct?");
    Serial.println("* did you change the chipSelect pin to match your shield or module?");
    while (1);
  } else {
    Serial.println("Wiring is correct and a card is present.");
  }

  Serial.println();
  Serial.print("Card type:         ");
  switch (card.type()) {
    case SD_CARD_TYPE_SD1:
      Serial.println("SD1");
      break;
    case SD_CARD_TYPE_SD2:
      Serial.println("SD2");
      break;
    case SD_CARD_TYPE_SDHC:
      Serial.println("SDHC");
      break;
    default:
      Serial.println("Unknown");
  }
  if (!volume.init(card)) {

    Serial.println("Could not find FAT16/FAT32 partition.\nMake sure you've formatted the card");
    while (1);
  }
  Serial.print("Clusters:          ");
  Serial.println(volume.clusterCount());
  Serial.print("Blocks x Cluster:  ");
  Serial.println(volume.blocksPerCluster());
  Serial.print("Total Blocks:      ");
  Serial.println(volume.blocksPerCluster() * volume.clusterCount());
  Serial.println();

  uint32_t volumesize;
  Serial.print("Volume type is:    FAT");
  Serial.println(volume.fatType(), DEC);
  volumesize = volume.blocksPerCluster();    // clusters are collections of blocks
  volumesize *= volume.clusterCount();       // we'll have a lot of clusters
  volumesize /= 2;                           // SD card blocks are always 512 bytes (2 blocks are 1KB)
  Serial.print("Volume size (Kb):  ");
  Serial.println(volumesize);
  Serial.print("Volume size (Mb):  ");
  volumesize /= 1024;
  Serial.println(volumesize);
  Serial.print("Volume size (Gb):  ");
  Serial.println((float)volumesize / 1024.0);
  Serial.println("\nFiles found on the card (name, date and size in bytes): ");
  root.openRoot(volume);

  root.ls(LS_R | LS_DATE | LS_SIZE);
  digitalWrite(chipSelect,HIGH); //disable device

  // BMP388 Initialization
//  if (! bmp.begin_SPI(BMP_CS)) { 
  if (! bmp.begin_SPI(BMP_CS, &SPI, 32000000UL)) { 
    Serial.println("Could not find a valid BMP3 sensor, check wiring!");
    while (1);
  }
  bmp.setTemperatureOversampling(BMP3_OVERSAMPLING_8X);
  bmp.setPressureOversampling(BMP3_OVERSAMPLING_4X);
  bmp.setIIRFilterCoeff(BMP3_IIR_FILTER_COEFF_3);
  bmp.setOutputDataRate(BMP3_ODR_50_HZ);
}

// **********************************************************************************
void loop(void) {
  if (! bmp.performReading()) {
    Serial.println("Failed to perform reading :(");
    return;
  }
  Serial.print("Temperature = ");
  Serial.print(bmp.temperature);
  Serial.println(" *C");

  Serial.print("Pressure = ");
  Serial.print(bmp.pressure / 100.0);
  Serial.println(" hPa");

  Serial.print("Approx. Altitude = ");
  Serial.print(bmp.readAltitude(SEALEVELPRESSURE_HPA));
  Serial.println(" m");

  Serial.println();
  delay(1000);
}