reComputer Industrial J3011 POE Camera on PSE Port

My 50 cents are that 192.168.0.117 is the IP of the Ethernet interface of the computer, not the IP of the camera. Sub 0.0 ms ping values are usually from the same device you are pinging from and the apache2 default page is from the reComputer itself.

What is the fixed IP configuration of the camera?