Rainbowduino Serial

So …
why dont you guys change the specifications then?
since seeedstudio only supports I2C on software, on the specifications it shouldn’t say:
“communications protocols: I2C, Uart”,
it should say I2C, possible Uart (ONLY hardware supported)
So It wont be so confusing …

I mean if you put Uart communication protocol, I woud expect that it would be a simple example on how to handle serial communication (by SeeedSatudio (full supported communication sample)), and with every process in the code commented. So if someone wants to change something quicly doesnt have to go through all the code to understand whats happening …

I am kind of frustating with this product because the official documentation v1.1 is not very clear and the code comments (besides it has quite of typos) is not very helpful,

thanks for the responses in the forum tho