Sorry if this posted twice.
okay, if it’s surface mount, is there an option of a socket for the MCU?
The reason I’m paranoid about burning out the MCU is that I want to work with higher voltage and opticouplers. I fear accidentally running 350vdc thru the board. I’m a novice, I don’t have experience with MCU and I don’t know if I will burn out the MCU or not.
Right now, I’m down to three candidate board: Seeeduino, Freeduino and…Illuminato (whenever the next batch of pcb is made).
I’ll decide over the weekend.
What is shipping to ship to Cleveland Ohio 44114 if I order the following items?
I believe I will be ordering (Still under consideration):
1 freeduino complete kit
1 Arduino ProtoShield kit remixed v1.0
1 20 in 1!Basic components mixed pack
1 315Mhz RF link kit
1 433Mhz RF link kit (Would 433Mhz be better than 315Mhz? what will 433Mhz offer me compare to a 315Mhz and 2.4Ghz?)
1 Breadborad jumper wire 75pcs pack
1 Basic Bread board - 17.1*6.2 cm
2 Mini Bread board 4.5x3.5CM
2 Infrared Remote Control Receiver Module
1 Digital Storage Oscilloscope DIY Kit with Panels) (not sure if I -need- an oxcilloscope???)
1 Pull the trigger! L135A Desoldering pump
2 6N137 High CMR high speed TTL compatible optocoupler
1 Rotary Encoder with Switch
1 5mm IR LED - 850nm 60 degree
1 5mm IR LED - 940nm
1 Original Osram IR LED - SFH485P
2 5mm Triple Output LED RGB - Common Anode
1 ATmega168-20PU (28-pin DIP) w/ Arduino Bootloader
thank you