Quad - Thoughts and Observations

Chai Xiao Guang is bure. So the e-Design DSOs are in fact the originals? Is bure the developer of both the hardware and the software? It would seem so as Seeed writes “Designed by Chai Xiao Guang” and the source is full of e-Design associations.
Maybe I went a bit to far in previous post, it was not meant as accusations, just pure thoughts. I also think it may be just that they are too fuzzy with the collaboration details. Seeed always talk in “we” form, not “e-Design” or “e-Design and we” so it is very unclear who did what. Most recent example seeed writes “but we over-clocked AD9288-40”. With dangerous prototypes they are more clear with texts like “we cooperated with some other firms like Dangerous Prototypes”. Seeed simply never talk about e-Design for some reason.