Has anyone actually got the 2 mic hat working on a zero 2? I have gotten to the point where i confirmed the kernel loading and sync’d The kernel header is visible and there’s where it ends. I have tried newest, legacy, and experimental kernels. I could match a header to the kernel but it wouldn’t load dtoverlay or the header was matched. That is two days work.