Problem BeagleBoneBlack + MotorBridgeCape

Hello,



Which image are you and your people using?







uname -a <<<< use this command to find out







The BBB and other variations run on another battery supply. Do not try to run both the Motor Bridge Cape and BBB off the same power supply.







The BBB runs off of 5v or 3.3v only. You can run your Motor Bridge Cape off a 12v 1.3 Ah lead acid battery.



Seth



P.S. If this is not the issue, please contact me. You may have to set up config-pin on specific pins so the Cape can communicate w/ the BBB. Once you have set up the config-pin utility, you may need to also figure out how to make the config-pin set up on boot or you will have to apply it each time in user space.