Post your wishlist of DSO firmware mutant

As probably one of the few “audio guys” who want to use this scope in the field when I was not expecting to need one…



It would be nice if the voltage could be interpreted in dBV or dBu with “0dB” being 1V or 0.775V rms. Also as someone posted previously a FFT would be really cool. I think it has also been suggested, but a higher input voltage (even if it is just over-voltage protection) in X1 would also help in a lot of situations.



I fully understand there are limitations to this little DSO - it is useful as it is!



Thanks for making a small and useful product!



Tim







EDIT: subscribed to thread.