Nrf52840 low power BLE consumption

The documentation you link is about the CPU. But there are more devices on the board, like the regulator and the sensors. All of them my consume some amount of current. You have to look at their data sheets and see, if they can be put into a low current state as well. Maybe a LED is still on, then it must be switched off. 250µa at 3v3 would be the current through a 13k resistor. So for a full populated board 250µs does not seem much. With a 2000mAh battery that would result in about a year stand-by time.