nRF52840 Error 0x800701B1

I don’t know what that means… BSP? what is that? I have never done anything with BSP…
Please do not assume I am an expert on this module.

I have just opened two BRAND NEW modules and I tried to program the uf2 file into the module. Both gave me the exact same error.
I am using:
adafruit-circuitpython-Seeed_XIAO_nRF52840_Sense-en_US-8.2.9.uf2

I drag the file into the XIAO-SENSE directory, it is supposed to program it and update it to CircuitPy.
Modules used to work for me in the past. Now, all of a sudden, this is happening.
If it matters, the modules were made in April and May 2024.

I never used to get an error when doing this. I do not trust these modules are working now.

If I look at a 3rd brand new board, without doing anything, the INFO_UF2.txt file on the device says:
UF2 Bootloader 0.6.1 lib/nrfx (v2.0.0) lib/tinyusb (0.10.1-293-gaf8e5a90) lib/uf2 (remotes/origin/configupdate-9-gadbb8c7)
Model: Seeed XIAO nRF52840
Board-ID: Seeed_XIAO_nRF52840_Sense
SoftDevice: S140 version 7.3.0
Date: Nov 12 2021

After programming the .uf2 file, when the error is generated, the CIRCUITPY directory appears with only one single boot file in it, that has this inside it:
Adafruit CircuitPython 8.2.9 on 2023-12-06; Seeed XIAO nRF52840 Sense with nRF52840
Board ID:Seeed_XIAO_nRF52840_Sense
UID:337E5A37BC92C7D2

I am pretty sure I had cleared out the CIRCUITPY folder which is why the only file was the boot file. The other module had all the contents of CIRCUITPY.