New XIAO ESP32C6!

For question 2, you can

Then, you would need to manually update the installed package with some missing parts, which are on the repository but not yet included in the Alpha 3 package. For example in Alpha 3, boards.txt does not list XIAO_ESP32C6, but the repository includes it.

Please take care in using LED_BUILTIN instead of 5 or 13 mentioned in the examples, as the numbers may interfere with the board and the boot-loader. Pressing the BOOT button saved me from a board without Serial.

The WiFi examples work fine. I faced building issues with the Bluetooth examples. I guess the Alpha 3 package still needs to mature.