NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!

Hi yokonav,



Thanks for your feedback.


  1. There is SWD interface already, so will not add ST-Link/V2-1 in this baseboard.
  2. Will try to replace the Lipo connector with a Grove connector.
  3. The Arduino Uno expansion will not be put on this board, otherwise, the board will be too complicated. Will breakout all the Arduino pin to Raspberry Pi 40-Pin, and provide a HAT with Arduino expansion.
  4. Yes, what STM32MP157C has is USB 2.0. USB3.0 is nice~ however adding USB 3.0 will add quite a lot cost, may consider it if there is a pro version.
  5. It is interesting to add NFC tag on a development board, do you have a specific application that needs this feature?



    Really appreciate and like the idea of “10 board”. I have suggested this name to our branding team. Thank you~