This development board seems really powerful and can serve many purposes.
I do not know if these are already planned but I would like to see:
- ST-LINK/V2-1 debugger/programmer
- Grove connectors (Seeed without Grove?)
- GPIO expansion connector (for Raspberry Pi shields) as well as Arduino Uno V3 expansion connectors (For Arduino shields). This double purpose board can take advantage from both of the worlds.
- USB 3.0 (it seems STM32MP157C supports USB 2.0 only but I may be wrong)
- NFC Tag (for provisioning, good for doing something without changing the code)
For the name I can suggest:
Since It is Seeed’s 10th Anniversary so “10 board”. The 10 is also a binary digit which is decimal 2 (basically it is two boards Linux+Arduino). “10” also looks like IO (input/output) or part of IOT. It is a catchy word which is good for branding.