Must re-flash meshtastic firmware after I upload Ardunio sketch

Hi there,

And welcome Back…

Why This Happens

When someone flashes a custom sketch (like an Arduino “Blink” or serial test) over Meshtastic firmware, they’re wiping out Meshtastic entirely. It’s no different than installing your own bare-metal firmware. That’s why afterward:

  • The device no longer shows up as TinyUSB or Meshtastic over serial.
  • It won’t respond to Meshtastic apps or commands.
  • It only boots your sketch — not the Meshtastic stack, not the radio, not the mesh.

So of course it looks “inaccessible” — you erased it.

So , you are overwriting the Meshtasic code on the xiao and it bombs?

What does the sketch look like ? Use the code tags and post it up “</>” paste it in there. Lets have a looksie :+1:
what is the end goal, I bet there is a different way to do it.

HTH
GL :slight_smile: PJ :v:

1 Like