Music Shield issues

I can get the code to compile and upload to the 2560 but that is where it stops. I bought this unit to play music and for sd storage on projects but, after plugging away on this and realizing the unit will not record without mega 1280, now I want to record. So when I went to buy a Arduino Mega they were sold out of the 1280 (so I bought a 2560). If I un comment the //Serial.println(“Hello test!”); the board will display serial info “Hello test!”. But no music or leds or button function. I also now get error messages only if I select the ATMega168 (not enough space). I feel so much better that I am able to use this now.

If I could help in any way to test revisions of code or if you have any suggestions for the 2560 to work please let me know. I can’t help but notice…
#if defined(AVR_ATmega1280)
is there any reason why changing 1280 to 2560 would help? I might just try to find a MEGA with 1280 to try. Does the Seeeduino Mega v1.1 work for recording?
Thanks!
Eric

By the way, the setup I have that worked is
Windows XP
Arduino Duemilanove w/ ATMega328
Arduino 22
noname 2GB sd micro