Hi,
I am also having a hard time getting a card to work.
I have a PNY 2G. I started by formatting it in my camera before I put it in my Nano. The Nano, says it has saved my settings, but it doesn’t. I am getting an SD error when I try to save a file.
I get the following when I plug the Nano in a usb port on my PC:
Jun 13 04:17:28 Cosmo kernel: [143962.757852] usb 4-2: configuration #1 chosen from 1 choice
Jun 13 04:17:28 Cosmo kernel: [143962.763835] scsi9 : SCSI emulation for USB Mass Storage devices
Jun 13 04:17:33 Cosmo kernel: [143967.762082] scsi 9:0:0:0: Direct-Access e-Design DSO Flash Disk 1.0 PQ: 0 ANSI: 2
Jun 13 04:17:33 Cosmo kernel: [143967.762530] sd 9:0:0:0: Attached scsi generic sg8 type 0
Jun 13 04:17:33 Cosmo kernel: [143967.767068] sd 9:0:0:0: [sdf] Unsupported sector size 1.
Jun 13 04:17:33 Cosmo kernel: [143967.767073] sd 9:0:0:0: [sdf] 0 512-byte logical blocks: (0 B/0 B)
Jun 13 04:17:33 Cosmo kernel: [143967.767076] sd 9:0:0:0: [sdf] 1-byte physical blocks
Jun 13 04:17:33 Cosmo kernel: [143967.770062] sd 9:0:0:0: [sdf] Write Protect is off
Jun 13 04:17:33 Cosmo kernel: [143967.775063] sd 9:0:0:0: [sdf] Unsupported sector size 1.
Jun 13 04:17:33 Cosmo kernel: [143967.780064] sd 9:0:0:0: [sdf] Attached SCSI removable disk
fdisk can’t handle it at this point either.
The card works fine if I plug it into a usb card reader.
So what’s the best way to get a card working in the Nano?