Relying to this topic because I canât seem to figure out how to create a new topic!?
I want to use the Wio-SX1262 Module in a project so I can leverage the module FCC certification but looking at the FCC approval it has three antennas an FPC, Spring and Diapole. It doesnât look like you all sell the FPC antenna that was used and the 2 dBi external antenna and SMA to I-PEX antenna cable one you do sell is not in the FCC approval. Am I missing something? I would like to buy a few modules with FCC approved FPC antennas. Thanks for any thoughts!
Adding to the post based on PJ_Glasso (thanks for replying!)âŚ
I am looking at the Wio-SX1262 with IPEX antenna connector for US market. I have a base that is powered and would like to put a 2 dBi external antenna like the one you all sell (External Antenna 868-915MHZ-2dBi;SMA-L195mm-Foldable) and then use the FPC antenna for the remote units (But I donât see you offering this antenna). I looked at the FCC report for the Z4T-WIO-SX1262 and it has three antennas but they donât really align with what you all sell except for the outdoor dipole. Is there someone that could provide some clarity on the situation, the goal would be to buy a FCC certified module and antenna based solution and then just do a certificate of conformity for the remaining simple circuit (I am definitely out of my depth on the FCC stuff but seemed to have read enough to feel somewhat comfortable with the options).