This may be the issue I am havin. Do you see how I’m configuring the Loras? It’s this line of code:
mySerial.write(“AT+TEST=RFCFG,868,SF7,125,8,8,14,ON,OFF,OFF”);
I have my GPS system on another Lora that operates of 915 MHz. The Lora for the deployment system constantly receives packets from the GPS (even though they are on separate frequencies). This is bad because the onboard system no longer is able to receive the arming command (I think it gets flooded from too many packets from the GPS interference. Please help this is really frustrating me.