Thanks for the infos, I’m not so surprised working a lot with Wifi systems for my customers and I noticed that very often antennas specs are “very” approximate
That’s why on gw I receive next week and I’ll setup on TTN, i’m going to exchange the basic spring style antenna supplied by a 2.8dB antenna optimised for Lora 868 (my band here) so it gets best coverage possible and I’ll update it in few weeks with a 5.8dB fiberglass antenna for the same band I’ll do some coverage tests in neighborhood once fully setup with TTNMapper so I cann check how it works (hopefully well
yep pretty amazed already how my sensor outdoor device still gets Lora cover while out of coverage and having far of the best antenna inside The counterpart of that very good range is probably the delay it takes to receive some paquets sometimes !
Thanks the info as I would have expected it that in current usage in the field but not on short coverage So no panic at first paquet not received