Join us, and Vote it!

Great to see that things are getting up and running. My first suggestion would be to enable clear communication, by allowing someone privileges to make changes to a post, or provide feedback on specific posts where their could be confusion due to grammatical or language errors. For example, I came across a phrase under the topic “Access the GPIO Pins based on Different IDEs” where, after the explanation for Arduino IDE for Rephone, under the image which attempts to provide some clarity, the phrase “This ain’t about rocket science, this is about making the difference.” to be very confusing; as the diagram has multiple ways this could be interpreted, if intended at all to be a reference to anything in the diagram.(Means Not Accessible) In yellow writing could be one of them…Anyways, if there was some administrators that could make changes to some grammar and phrases to provide more clarity in certain places I think it would be great…
Can’t wait to see what things look like in a year, keep up the good start…
YellowCake