Actually, as I mentioned above, the code is working for the combined UV / Temp & Humidity sensors. I could use your guidance on the integration of the Air Quality sensor as the code structure is a bit different with a class definition included in the script.
indent preformatted text by 4 spaces
#!/usr/bin/env python
# -*- coding: utf-8 -*-
#
# The MIT License (MIT)
#
# Grove Base Hat for the Raspberry Pi, used to connect grove sensors.
# Copyright (C) 2018 Seeed Technology Co.,Ltd.
'''
This is the code for
- `Grove - Air Quality Sensor <https://www.seeedstudio.com/Grove-Air-quality-sensor-v1.3-p-2439.html)>`_
Examples:
.. code-block:: python
import time
from grove.grove_air_quality_sensor_v1_3 import GroveAirQualitySensor
# connect to alalog pin 2(slot A2)
PIN = 2
sensor = GroveAirQualitySensor(pin)
print('Detecting ...')
while True:
value = sensor.value
if value > 100:
print("{}, High Pollution.".format(value))
else:
print("{}, Air Quality OK.".format(value))
time.sleep(.1)
'''
import time, sys
from grove.adc import ADC
__all__ = ["GroveAirQualitySensor"]
class GroveAirQualitySensor(object):
'''
Grove Air Quality Sensor class
Args:
pin(int): number of analog pin/channel the sensor connected.
'''
def __init__(self, channel):
self.channel = channel
self.adc = ADC()
@property
def value(self):
'''
Get the air quality strength value, badest value is 100.0%.
Returns:
(int): ratio, 0(0.0%) - 1000(100.0%)
'''
return self.adc.read(self.channel)
Grove = GroveAirQualitySensor
def main():
from grove.helper import SlotHelper
sh = SlotHelper(SlotHelper.ADC)
pin = sh.argv2pin()
sensor = GroveAirQualitySensor(pin)
print('Detecting ...')
while True:
value = sensor.value
if value > 100:
print("{}, High Pollution.".format(value))
else:
print("{}, Air Quality OK.".format(value))
time.sleep(.1)
if __name__ == '__main__':
main()