Well that did not work. Mac has:
- Python 2.7.16
- Python 3.8.6
- Pip 18.1 from /Library/Frameworks/Python.framework/Versions/3.8/lib/python3.8/site-packages/pip (python 3.8)
BUT as part of the install I get:
ardupy-aip 0.8.1 requires pip>=20.1, but you’ll have pip 18.1 which is incompatible.
So upgrading pip to 20.1 with sudo -H python3 get-pip.py pip==20.1 gives a different error:
ModuleNotFoundError: No module named ‘requests’
but a quick sudo -H pip install requests gives me an aip command that does not error on the help!
So it looks like the process is:
- Install Python 3 on the Mac from python.org
- Download get-pip.py
curl https://bootstrap.pypa.io/get-pip.py -o get-pip.py - Run that to install version 20.1
sudo -H python3 get-pip.py pip==20.1 - Add the ‘requests’ module using pip
sudo -H pip install requests
This MAY work in a virtual env but I’m not testing that til 2021.
FORGET IT - the next thing I try dies with
FileNotFoundError: [Errno 2] No such file or directory: ‘/Users/andrew/.config/aip/modules’
Going to ask for working instructions from the devs.