Here’s the output
20:34:52.032 -> Master UID 5F9F613
20:34:52.032 -> ******** verify=1
20:34:52.032 -> // run the reset sequence
20:34:52.070 -> // return immediately when verification is disabled
20:34:52.070 -> // set mode to standby - SX126x often refuses first few commands after reset
20:34:52.070 -> // try to set mode to standby
20:34:52.070 -> standby() standbyXOSC=0
20:34:52.070 -> standby() mode=0 wakeup=1
20:34:52.070 -> // set RF switch (if present)
20:34:52.070 -> // pull NSS low to wake up
20:34:52.070 -> SPIwriteStream RADIOLIB_SX126X_CMD_SET_STANDBY