How to install Docker on ReSpeaker V2?

This little elegant case is probabaly the most suitable case which you can get for ReSpeaker. The design is compact while at the same time provides enough space for one ReSpeaker core plus one ReSpeaker Far-field MIC array. There isn’t much ornament except the rounding aperture that makes your voice more reachable and the translucent circular ring that indicates the light being generated from the ReSpeaker inside. ReSpeaker Core v2.0 is designed for voice interface applications. It is based on the Rockchip RK3229, a quad-core ARM Cortex A7, running up to 1.5GHz, with 1GB RAM.