How to debug Xiao Seeed nrf52840 through NRF52840 DK

Hi there,

You should probably go and watch the Video on adding a build configuration (youtube) I don’t see yours? why only System builds? Did you create a New Board ?
Let me switch toolchains and get back, Probably because there’s no board defined in the BUILD ? 'm guessing or its just a copy of the DK system build?? either way it’s not what you want. Are you using a Xiao Dev board ? Is it configure the same as what I posted ?

So if you power off the Xiao Dev Board does the NRF52840 change to _xxAA_REV3 ?
when you refresh the dev board?
Start with the basic’s doesn’t matter if you can flash it , as that’s going to be required to debug anyway. :+1:

When you create the build .conf do you see it find the device board file? “Xiao_ble”

LMK

HTH
GL :slight_smile: PJ :v:

the more I look at this , If you can debug the DK builds, Then the answer is in between the build files and the Board files.
Also besure the toolchain MATCHES the SDK version… :+1:

Here is the VB About info , What’s is yours?

Version: 1.96.2 (user setup)
Commit: fabdb6a30b49f79a7aba0f2ad9df9b399473380f
Date: 2024-12-19T10:22:47.216Z
Electron: 32.2.6
ElectronBuildId: 10629634
Chromium: 128.0.6613.186
Node.js: 20.18.1
V8: 12.8.374.38-electron.0
OS: Windows_NT x64 10.0.26100