Help with CircuitPython

Can anyone help with this? The specs say this board should have 256KB flash but somehow I only have 66KB available. The total files that I’ve added to the board are only just over 8KB yet somehow the disk is “full”. I’ve checked for hidden files (both by enabling viewing of hidden files and looking on the command line), but nothing seems to be there.

This is making development troublesome because I can only add a couple of library files before I run out of space. Is there any way I can possibly enable or access more disk space on the CIRCUITPY drive?