Ok, Try this with the delay’s…
// Sunlite..
#include "Si115X.h"
Si115X si1151;
/**
* Setup for configuration
*/
void setup()
{
Serial.begin(9600);
delay (2000);
Wire.begin();
delay (500);
if (!si1151.Begin(0x53)) {
Serial.println("Si1151 is not ready!");
while (1) {
delay(1000);
Serial.print(".");
};
}
else {
Serial.println("Si1151 is ready!");
}
}
/**
* Loops and reads data from registers
*/
void loop()
{
Serial.print("IR: ");
Serial.println(si1151.ReadIR());
delay (500);
Serial.print("Visible: ");
Serial.println(si1151.ReadVisible());
delay(500);
//Serial.println(si1151.ReadUV());
//delay(500);
}
Lmk,
So , I’m down to Defective device?, or the wire lib is broken, or needs 2wire.lib ?
more info needed, Can you post a pic of the Hardware setup?
HTH
GL
PJ