Grove NFC v1.1 does not work with UART

Sorry for hijacking this post.

I am using the Seeeduino Yun with the NFC Grove 1.1
I installed the library following the Seeeduino wiki page ( Grove - NFC | Seeed Studio Wiki) and flashed the sketch from the example (read tag), which is the same as you have posted.

The serial monitor is showing nothing. I checked into the code. It is because the code hangs in following snipet (NfcAdapter.cpp).

I commented out the while loop, but then the uint32_t versiondata = shield->getFirmwareVersion() returns zero.
Any ideas?

void NfcAdapter::begin(boolean verbose) {
…
if (! versiondata) {
#ifdef NDEF_USE_Serial
Serial.print(F(“Didn’t find PN53x board”));
#endif
while (1); // halt
}

Just an update:
I figured it out by using software serial. Tag read/write is working now