inline float calcVol(uint32_t adc) { return (adc * 3.3) / GM_RESOLUTION;
Q1. Is this the Vs voltage?
Q2. What is adc? It is not defined anywhere.Q3. If the output voltage is Vs, then,
Rs = (Vc-Vs)/Vs, where Vc = 3.3 V. Is this correct? (is it like in MQ9 sensor?)
Hi, im having some similar issue…
about Q2… abc is defined as a param of calcVol function. inline float calcVol(**uint32_t adc**) {
did you resolve the high values on measurements?