Hi yurip,
Sorry, I don’t get what you said “You can connect to PC serial port directly first.” I already tested GPSBee with PC directly (ie: via MAX232). Or directly connect PC serial port with GPSBee module (without MAX232)? Are you kidding me .
And also tested outdoor about 45mins but nothing changed.
I also test with realterminal (www.u-blo$GPTXT,01,01,02,u-blox ag - ".
I also tried to change PIN-15 setting 1 and 0. According to data sheet, it should work with 1Hz update and default UART speed 9600ps without using this pin.
For MAX232, it should be work with any UART enabled device.
Thanks for quick reply.