i seem to remember a portion of the code that required the TFT_eSPI to be commented out //
that may have to do with it too
ps i think on windows if you go into my documents - arduino folder - libraries you can delete offending instalations… but also sometimes the folder is not the same name as the offending file
also during compile error you can see the offending path
windows no longer allows the setup of “dummy users” to separate login
but maybe on lynix you can set up a new login and get a clean install of arduino without having to wipe the whole OS
regards