Getting Started with Seeed Studio Round Display for XIAO | Seeed Studio Wiki

For those looking for the datasheets of the screen and touch controllers, see 240x240 Round IPS TFT LCD Display 1.28" Capactive Touch Circle Screen at Buy Display.

Notable differences are:

  • Screen GC9A01A SPI controller: SPI MISO is not implemented on the screen, so reading a pixel is not possible.
  • Touch CST816S I²C controller: automatic low power mode is on, direct read gives 5 bytes for number, event, x, 0, y.

Enjoy!