Getting Started with Seeed Studio Round Display for XIAO | Seeed Studio Wiki

Thank you! The hardware test compiled! Now I am waiting for the Round Display to arrive. It should be here before week is out. It is being handed over to USPS now.

Can I ask a question regarding reTerminal E10-1 (bridge)? I finally found a M.2 SATA III (could not find any SATA II) and it works but after formatting and mounting, I have no permission to use it. I am hoping chmod will fix it. But the real question is the battery power. Installed two that match the specs (Flat tops) and charged the batteries before installing. Should I be able to power up the reTerminal via the E10-1 batteries? If so, it is not working. The 12V adapter powers both the bridge and the reTerminal but not the batteries?

Reference for the M.2 SSD: TEAMGROUP MS30 512GB with SLC Cache 3D NAND TLC M.2 2280 SATA III 6Gb/s Internal Solid State Drive SSD (Read/Write Speed up to 530/430 MB/s) Compatible with Laptop & PC Desktop TM8PS7512G0C101