Peripheral were placed on the metal railing of the second floor window. Central was mounted on XIAO Expansion Board so that RSSI could be observed on the display, and moved a little further away to measure the distance at which the connection was broken. The metal rail might have the effect of reinforcing the antenna. Tomorrow I will experiment with non-Sense XIAO.
1 Like