Getting lower power consumption on Seeed XIAO nRF52840

Hi everyone! I’m here looking for some advice because my Seeed XIAO nRF52840 are using 1.8 mA in deep sleep. I want to power them using coin cells so that’s a problem because I’d be using one up in a matter of days instead of several months.
I used the code by @PJ_Glasso to toggle between awake and deep sleep using two buttons and I tested it on all three devices. They are using 4.3 mA awake and 1.8 mA asleep. Before trying the button solution, I ran the code from this thread Sleep Current of XIAO nRF52840, Deep Sleep vs. Light Sleep and got the same result, except the first time I did it on the second device it only needed 8µA. I tested the third, which also needed 1.8 mA (actually 1.9 mA that day but that could just be the multimeter). When I went back to the second device it then also consumed 1.8 mA and does so ever since. I am not sure what’s going on there. What can I do to investigate the root cause? I am a decent programmer and have some knowledge of electric circuits, but when it gets down to electronics know-how that I read here by people that squeezed out the last microamps I am lost. I’ll do my best to follow but please dumb it down if possible.

My device information is the same as already given above:
UF2 Bootloader 0.6.1 lib/nrfx (v2.0.0) lib/tinyusb (0.10.1-293-gaf8e5a90) lib/uf2 (remotes/origin/configupdate-9-gadbb8c7)
Model: Seeed XIAO nRF52840
Board-ID: Seeed_XIAO_nRF52840_Sense
SoftDevice: S140 version 7.3.0
Date: Nov 12 2021

I use the Arduino IDE and it shows up with the suffix Sense there for whatever reason.

Cheers, Daniel

https://www.amazon.com/URGENEX-Battery-Rechargeable-Batteries-Quadcopter/dp/B08XZNRTCP/

Hi dt10,
The sketch in the link below should be able to reproduce the uA sleep current. Is your multimeter good enough to measure uA? Tell us about your experiment in detail. When did you say the current was 1.8mA, @PJ_Glasso’s sketch? Or @msfujino’s sketch?

Hi there,
and welcome here.

Pay attention to the BSP (board support package) and weather your using the non-mbed or mbed versions on the BSP’s. We use the power profiler to collect the power Info you see.
The Power Ninja @msfujino :ninja: is the most experienced with this topic hands down.
So I can only add ," what he said" :grin: :open_hands:

take your time and read EVERYTHING you will get up to speed no problem. come here and post any questions,and code using the code tags above(</>) paste it in there, pictures hepl to, lots of very helpful smart people are present most days & nights :stuck_out_tongue:
I have used coin cells on Xiao no problem. I like these cr-2450’s


they are a little fatter…(thicker).

HTH
GL :slight_smile: PJ

FYI, there are things like shutting down or sleeping the external Flash also will lower the sleep number. It’s great hardware and sometimes the software dev lags but the user base holds it down and parallel devs like adafruit and nordic add to the knowledge base.
What is your end vision with this? :+1:

here is the latest from me…
Getting lower power consumption on Seeed XIAO nRF52840 - #59 by PJ_Glasso

Thank you both for getting involved! I get the same result from both @msfujino deep sleep and @PJ_Glasso post #59 sketches.

Here is my current setup. The board with the red LED that connects to the USB Li ion battery is a boost converter where I removed to outgoing USB port and put pins in its place. Sorry if this butchering of the board hurts your eyes, I suppose it does. I know I could directly go from the USB port of the battery, but due to the pins the boost converter was the easiest way for me to enable the current measurement without cutting up another USB cable*. To measure the current, for lack of better equipment, I used those two clips to connect the multimeter on the high side. I have to push buttons connecting to ground on D2 and D3 and ground and 5V on the respective pins, nothing else

…oh no, it says I can’t embed media!.. let me try dropbox links to the pictures… you’ll have to click them because it only shows those broken image icons, sorry about that!

Board support package, BSP, thanks for spelling it out for me! This is what I got. I hadn’t noticed that it picks the “Sense” by default, but I just repeated the measurement after selecting non-sense and it did not make a difference.

Daniel

*in case you are wondering what is going on there: I am using two of the XIAOs that communicate using BLE. After developing both sides of the code I used this boost converter with a CR2032 to test things. I made a rookie mistake in the BLE code and I think that drained the coin cell quickly. To prevent that for further testing, I put the USB C cable in place so that I can use that Li battery and keep using the pin strips. If you are thinking why on earth did he keep the boost converter, it’s because I also wanted to measure how much current it can provide because the data sheet said “500 to 600 mA” and I wanted to know.

Hi there,

Nah’ :face_with_peeking_eye: Looks like a WIP to me :+1:
You do what you can do, with what you got, No Shame in that game! (post limit will lift and you can post pics after a few posts, btw) I see the Dropbox files. :wink:
SO what I see is your NOT using the battery connections on the bottom of the Xiao? Why NOT?
All bets are off if you choose to not power it that way, the other methods require a diode and
other considerations and will NOT get the LOW numbers NO-WAY!
Yada, yada , Boooster , Buck converter it’s all been done before not a big deal.
(honestly I LOL because all the first attempts are like yours , me included and look this way…WRONG..LOL!) :laughing:
the smaller CR2032 coin cells will get you 350-450 ma. run time current total then it’s down hill and done from there. I like the 2450 has more juice longer and supports more total power draw.
During the advertising phase of the BLE the Xiao uses the most current. so the Idea is do the (setup) heavy lifting for the connection right away and then go Sleep. “rinse and repeat”
mind you many optimisations can be made to the BLE connection parameters and settings to squeeze the max out of battery life.
In your code if you are using the Serial port or “while Serial” the port will wait until a USB cable is connected and the rs232 driver/rec 1488/89 are in MARK state and using 1.x ma. of current.
Have a look at the schematic for the Xiao and READ the Links to @msfujino :ninja:
research on “System on SLeep”

BSP… Board Support Package there are two Mbed versions (2.9.1) & NON-mbed versions(1.1.1) to start with.

have you gone over this: ?

Are you SURE you read the Wiki?

Two Arduino Libraries​

Seeed Studio XIAO nRF52840 assembles many functions in one tiny board and sometimes may not perform the best of them. Hence, Seeed has published two Arduino libraries to let it maximum the power of each function. Therefore:

  • It is recommanded to use the Seeed nRF52 Boards library if you want to apply Bluetooth function and “Low Energy Cost Function”.
  • It is recommanded to use the Seeed nRF52 mbed-enabled Boards library if you want to use it in embedded Machine Learning Applications or apply “IMU & PDM advanced function”.
  • Both libraries support very well when it comes to the basic usage, such as LED, Digital, Analog, Serial, I2C, SPI.

The Pin definition supported by these two libraries might be a little different and Seeed will keep update the wiki until it is clear.

Stop and take the time to RTFM :smile: is the best advice your close but your missing the basic understandings it will clear it up or generate the right questions to help you.
then you can get these:



LINK

HTH
GL :slight_smile: PJ :v:

Hi PJ!

Yes, of course I read the getting started, down to the battery charging which is not something I plan to do. I would not have known how to get it running in the first place without it.

Why not the battery pins? I, as I now know mistakenly, thought I can just as well use the pins for that purpose and since I already did the pin strips I went with that. I just soldered wires to the battery pins and now it’s working. When it wakes up I briefly see 100-something µA on the multimeter before it settles to 18 µA. In sleep mode I get 3.5 µA, so both readings agree well with your detailed measurements. Thanks PJ!

I am looking forward to merging this with the BLE code and the ADXL345 (to wake up the device due to being used) and see how low I can go. I am sure there will be some more surprises along the way but the individual parts are working. If I had realized there’s a version with motion sensors I would have bought that one. My ADXL345 board requires about 60µA, which isn’t great but if I manage the interrupt wake up working with the 1Hz or 8Hz sleep mode I hope this will go down. The BLE part is only notifying values at the push of buttons. Measurements will tell, but I think I did a reasonable job there.

Thanks again!
Daniel

Thinking about it, maybe I won’t even need the motion wake-up on this side of the BLE communication. If I can make it wake up on pushing the button and then notify it would be sufficient. I already see myself programming half the weekend :sweat_smile:

Ok, now that wasn’t the most productive weekend, or Monday. I still tried the motion sensors to determine when it is time to go to sleep and when to wake up together with BLE communication because I have other uses for it. It took some time, but it worked nicely. Nevertheless, for such a coin cell powered application where all I want to do is (briefly) send which button has been pushed when one is pushed and then go back to sleep, I wanted to do wake up → advertise (specifically a beacon where I placed the button number) → return to sleep after a prescribed time has passed. But I had not considered an important aspect of deep sleep, which is that on waking up it starts all over. It’s probably plain that I am relatively new to all this, but what I learned about using interrupts was that they are supposed to communicate to the main code using volatile variables. That doesn’t work in the waking up scenario when it starts from a reset. So my question is, is there a way to determine that the device woke up due to an external interrupt and where it came from? I searched but I didn’t find an answer (or did but failed to realize it). Because if there isn’t, I will have to try my luck with system ON sleep. I already read the thread today and found that my battery pins mistake was actually discussed there.

Regards,
Daniel

Hi there,
So i think take a look at the Technical reference guide for the Nrf52 part. I’m sure it is addressed in there, the other is using the Flash memory to tell the boot count and if it is awake, Also there is a wakeup Stub that runs a certain setup stub when waking up, AFAIR

also, You wouldn’t know if the advertisement is seen or not too that way I would look for another method with a Notify or some feedback, that way you can maximize your sleep counter and not wake premature to being required to (sensor update or x?). if that makes sense

HTH
GL :slight_smile: PJ :v:

All of it is GOOD stuff :+1:

I read a couple of things at Nordic but I concluded that this is too advanced for me right now. I only started with an Arduino starter kit a bit more than a month ago and still lack the level of knowledge about what is going on “behind the scenes” to make sense of what I read there. Until I feel confident that there is a good chance of success making this work, I will use the system ON sleep! This gives me 22 µA while waiting and about 130µA for a second when advertising at the push of a button. That gives me about a year from a CR2032. Crazy! I may even add deep sleep after an inactivity period and use an initial button press as an on-switch and it will last years.
On the scanning end, I have deep sleep with ADXL345 wakeup (and a 18650 battery so power is not really a huge concern). This has become obselete because my ADXL345 board needs 60µA, so I would be better off with system ON sleep. At least I learned something while developing it!

About the BLE, the beacon worked in testing. I can revisit more elaborate communication if I turns out to be unreliable in practice. I already have done it before using notify in code that I derived from the custom_hrm example. I will revisit that if I am not satisfied with the performance regarding a quick succession of button events. But first, onto the next problem. I have two buttons working, but I might like to have three and there’s only two straightforward interrupt pins. After this I draw a line! :sweat_smile:

So I read that some of the interrupt pins use more power if latched or if Edge vs, level for the interrupt to be generated there’s that and also if you use the pull up or pull down during sleep.

When I encountered a high than expected power consumption, I deactivated most code and started uncommenting and measuring. In system ON sleep and deep sleep without anything else active, the current is 5µA or 3µA respectively. When I set a digital pin to INPUT_PULLUP, this goes up by 31µA. The additional current is independent of the number of INPUT_PULLUP pins (I tried D2, D3 and D4, same as with just D2). Why is that? Is that the current needed by a give or take 100 kOhm resistor at 3.3V and there is no way around that? Meaning I can sleep for 3µA but need another 30µA to be able to wake up again?

Hi there,

yes, You will find it in the “technical reference Guide” it is the more in depth info about the actual silicon. You probably then want to use a timer to wake up. No pull-up required.
HTH
GL :slight_smile: PJ :v:

Try this sketch.
You can connect an external 3k3 pull-up or pull-down resistor if needed.
Sleep current is about 2uA when 3.8V is applied to the battery pad.

//----------------------------------------------------------------------------------------------
// BSP : Seeed nRF52 Borads 1.1.8
// Board : Seeed nRF52 Borads / Seeed XIAO nRF52840 Sense 
//----------------------------------------------------------------------------------------------
// 2025/01/15

#include <Adafruit_SPIFlash.h>    // 4.3.4, NOTE:need to deleted /Documents/Arduino/libraries/SdFat
#include <flash_devices.h>

// for flashTransport definition
Adafruit_FlashTransport_QSPI flashTransport;
Adafruit_SPIFlash flash(&flashTransport);
static const SPIFlash_Device_t my_flash_devices[] = {P25Q16H,};
const int flashDevices = 1;

#define PIN_WAKEUP (28)  // D0:(2), D1:(3), D2:(28), D3:(29), D4:(4)

void setup()
{
  // Enable DC-DC converter Mode
  NRF_POWER->DCDCEN = 1;            // Enable DC/DC converter for REG1 stage
  
  // on board Flash enter to Deep Power-Down Mode
  flash.begin(my_flash_devices, flashDevices);
  flashTransport.begin();
  flashTransport.runCommand(0xB9);  // enter deep power-down mode
  delayMicroseconds(5);             // tDP=3uS
  flashTransport.end();

  // Light Sleep Mode (RTOS delay function)
  delay(1000);

//  sd_power_gpregret_set(0, 0x6D); //Set GPREGRET0 to 0x6D (DFU_MAGIC_SKIP)
//  nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLDOWN, NRF_GPIO_PIN_SENSE_HIGH);
  nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLUP, NRF_GPIO_PIN_SENSE_LOW);

  // Deep Sleep Mode
  NRF_POWER->SYSTEMOFF = 1;
}

void loop()
{
  // nothing to do
}

Not on my device! :confused:
In that sketch, P25Q16H is not defined. I used this from your Flash_Light_Deep_Sleep example:


SPIFlash_Device_t const P25Q16H {
  .total_size = (1UL << 21), // 2MiB
  .start_up_time_us = 10000, // Don't know where to find that value
  
  .manufacturer_id = 0x85,
  .memory_type = 0x60,
  .capacity = 0x15,

  .max_clock_speed_mhz = 55,
  .quad_enable_bit_mask = 0x02, // Datasheet p. 27
  .has_sector_protection = 1,   // Datasheet p. 27
  .supports_fast_read = 1,      // Datasheet p. 29
  .supports_qspi = 1,           // Obviously
  .supports_qspi_writes = 1,    // Datasheet p. 41
  .write_status_register_split = 1, // Datasheet p. 28
  .single_status_byte = 0,      // 2 bytes
  .is_fram = 0,                 // Flash Memory
};

With your sketch and this definition it’s at 4µA in the light sleep mode. I increased the delay to 10s just to be sure I have plenty of time to take the reading because I only have a multimeter. When it goes into deep sleep after defining the wake up, it takes 31µA. When I comment out the nrf_gpio_cfg_sense_input line it sleeps at 2.1µA. This is exactly the same behavior I got with my own testing sketch, but that wasn’t unexpected because I derived it from your Flash_Light_Deep_Sleep sketch and just added some LED blinking to know when what is happening and the nrf_gpio_cfg_sense_input to be able to wake up the device.

Hi there,
What is your measured VCC? 3.6Vdc to 3.85 Vdc ?

GL :slight_smile: PJ :v:

Your situation is probably different from what we imagine. I ask you a few questions to help us resolve the issue quickly.

  1. Is the Board Support Package version 1.1.8 ?
  2. Is the “Adafruit SPIFlash” library version 4.3.4 ?
  3. What is the pin name (e.g. D2) used for wake-up? And what is connected to this pin?
  4. Please tell us everything that is connected to the XIAO pins without omitting anything. If possible, a connection diagram would be helpful.
  5. Please post your sketch.

The internal pull-up resistor of the nRF52840 is 15k. This means that about 31u-2.1u=29uA of current is passing through the pull-up resistor and out through the wake-up pin. Is something of about 3.3-29u*15k=2.9V connected to the wake-up pin?

I got 3.15V on the 3.3V pin and 0V on the 5V pin.

  1. Yes, version 1.1.8
  2. I checked in the library manager and it said Adafruit SPIFlash was not installed. I installed it, then I got a complaint from the compiler about multiple libraries. From this I found that version 4.2.0 was installed in AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries. I also have the SdFat directory that is mentioned in your comment there and was also installed along with 4.3.4
  3. D2
  4. Nothing is connected anywhere except a CR2032 to the battery pins.
  5. I propose to stick to yours from post 73 to keep better focus because if it works for you but not for me there’s nothing to gain by introducing additional variables.
    With 4.3.4 installed and used, P25Q16H seems to be known because I was getting a compiler error when I had inserted the definition I posted previously. It seems that it was using the SdFat library from the AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries installation alongside the 4.3.4 I installed and I still got those 30-something µA reading. I removed this SdFat directory as well and the compiler gave me an error:
c:\Users\User1\Documents\Arduino\libraries\Adafruit_SPIFlash\src/Adafruit_SPIFlash.h:32:10: fatal error: SdFat.h: No such file or directory
   32 | #include "SdFat.h"

There are two error checks relating to SdFat in Adafruit_SPIFlash.h, so simply commenting out the #include statement is not enough. Did you modify the library to get it to compile?

Found SdFat_-_Adafruit_Fork 2.2.3 in /Documents/Arduino/libraries/. Try installing it from the library manager.

If nothing is connected other than the battery, I don’t think the current consumption will increase just by pulling up.
You could try pulling up D0 to D10 in sequence and check if the problem is caused by the location of the pins. Another thing, why don’t you check if the soldering of the pins is incomplete and not short-circuited to anything.

The rated current of CR2032 is 0.2mA, which is too inefficient to start nRF52840.
Can you try with a 3.7V LiPo battery?

I checked the compiled output and the following file was used for SdFat. \Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries\SdFat

Thank you for thinking this through! I checked visually and then also with the multimeter already this morning. There are no shorts between pins. I have now tried with SdFat_-_Adafruit_Fork 2.2.3, same behavior. When I switched from D2 to D3, it started to reset constantly. I did not add a pause to verify yet, but I think it is instantly waking up again after going to deep sleep. I still have the other device which is wired for my application where I originally observed the 30+ µA. I can also check with this one because maybe my testing one is damaged. That’s something for the weekend though, need a break after work today!

I can also try a stronger battery, but at least the Duracell CR2032 is rated for 20mA/1 sec. I am not allowed to post links though, so you’ll have to believe me. I couldn’t find values for the Varta cell that I have, but I suppose it similar and there’s been no problem using it for BLE things.