I followed the guide many times.
The problem i mentioned happens when flashing the orin nano for the second time, this applies for all three boards i own.
when flashing the board for the first time I use the command provided in the guide, but after that i have to use the command i provided earlier with board id, board sku, fab, chip_sku
JetPack 6.0, but does not related to only 6.0 i tried the older versions with same issue 5.1.1 and 5.1.2
as i said earlier the main issue is that EEPROM is empty after first flash, and that’s what should be fixed
thanks