ESPHome and Seeed XIAO Round Display - will these work with ESPHome?

PJ,

Thank you for this - yes this is what I was using for reference. Looks an awesome project, and uses a screen and ESP32 from AliExpress.

I was trying to recreate this using Seeedstudio Round Display and one of their XIAO ESP32-C3 boards which attach to the display. Perfect I thought…

So I tried to reference the pinouts from the display and ESP board and add the GC9A01A display model from the ili9xxx platform.

So what I don’t understand is:
1 - are my pinouts correct for this combination of board + display module
2 - has anyone else got this working using ESPHome
3 - is the GC9A01A able to be used in this way?

Thanks

Tim