Thank you for your reply - I did get the demo working with Arduino IDE following the instructions, but I was hoping to use ESPHome within Home Assistant and leveraging the GC9A01A driver from the ili9xxxx platform.
I can’t get the display to do anything (I know it works) so I must either have the ports incorrect, or the GC9A01A isn’t the right driver for the display. There are other example of others using the GC9A01A with ESPHome and some of the config I am using is from these examples. The difference is the Seeedstudio packaging potentially, or it not being compatible with ESPHome as all the Seeed examples are for Arduino IDE.
Any ideas, or should I give up getting this to work with ESPHome and use PlatformIO or Arduino IDE?
Thanks
Tim