Hi there, Can I make a suggestion, Have you tried using 2.0.8 BSP?
LMK
GL
PJ
can you provide the compiler output from the build first 20 lines and last 20 lines would be sufficient
TIA
Hi PJ,
Nope, I even didn’t know such a thing exists. Looks like Seeed Studio’s ESP32S3 is not supported according to this.
TVM.
Hi there,
No It is , They use the Variant listed int the Table from the link in that Github wiki, Bottom of page.
However Seeed Studio Should make a concerted effort to get them recognised in Arduino , PlatfronIO and IDF and the nordic SDK. IMO
HTH
GL
PJ
In arduino IDE you can select a version prior to the Alpha, I tried using 2.0.8 and the attached code, I don’t have the WebSocketCleint.h version?
Have you tried it on an Xiao ESP32C3 ?
Add this code before while loop in setup function to print out near wifi check if it discovered wifi or not
// WiFi.scanNetworks will return the number of networks found
int n = WiFi.scanNetworks();
Serial.println("scan done");
if (n == 0) {
Serial.println("no networks found");
}
else {
Serial.print(n);
Serial.println(" networks found");
for (int i = 0; i < n; ++i) {
// Print SSID and RSSI for each network found
Serial.print(i + 1);
Serial.print(": ");
Serial.print(WiFi.SSID(i));
Serial.print(" (");
Serial.print(WiFi.RSSI(i));
Serial.print(")");
Serial.println((WiFi.encryptionType(i) == WIFI_AUTH_OPEN)?" ":"*");
delay(10);
}
}
Xiao esp32 s3 come with antenna. You have antenna on it or not?
Hello faizannazir,
Thanks for your answer. I was late to answer sorry for that.
Yes, I use the antenna of course.
I uploaded the code you gave me and it did not work as well.
I keeps disconnecting.
I think it is because the driver of the microcontroller is corrupted. How can I upload a new driver for XIAO ESP32S3?
Thanks a lot.
maybe wifimulti library causing issue
Hi there,
If you mean to reload the Factory bin file it’s here on the WiKi
ESP_RF_Test tool is used to flash it to the chip.
If memory serves me the tool ALSO has a Factory Flash file present.
HTH
GL
PJ
you guys crack me up…
Hi PJ,
Imma give it a try thanks a lot.
Have a great day.
Hi waltney,
Yes, I do not know how these work properly so I am struggling ![]()
Have a nice day.