ESP-AT Lib Initialisation Failure

And that worked - I am now seeing the SSIDs using the scan program.

I downloaded the uf2 update and firmware again as well as the flashing tool.

The uf2 update seemed to run as before.

I ran the erase again - this time it did seem to take longer than I remember from last week.

I used the command line that BoRRoZ provided, changing the directory names and COM port number.

.\amebad_flash_tool.exe flash -d C:\flash\20200730-rtl8720d-images-v2.2.0.2 -p COM8

After downloading the scanning program from the IDE, the device momentarily went into download mode (the D:Arduino popped up) and then disappeared again. Then the scan started working, showing the SSIDs in the serial monitor.

I’m not sure where I went wrong before but I am really grateful for everyone’s help and patience with this one.

For completeness, this is the log.

PS C:\flash\amebad_flash_tool_v0.1.0_windows> ./amebad_flash_tool erase -p COM8
Erasing…
All images are sent successfully!
Image tool closed!
done!
PS C:\flash\amebad_flash_tool_v0.1.0_windows> .\amebad_flash_tool.exe flash -d C:\flash\20200730-rtl8720d-images-v2.2.0.2 -p COM8
copy img to workspace…
Flashing…
All images are sent successfully!
Image tool closed!
done!
PS C:\flash\amebad_flash_tool_v0.1.0_windows>

Now for MQTT!

Allan