Error using Temperature and Humidity sensor v1.2

Hi there,



I got the sensor yesterday and final get it work. I used the latest raspberry image(2018.6.27). then i run below command to install grovepi.



sudo curl -kL dexterindustries.com/update_grovepi | bash

sudo reboot



at last, i run below commands and it is the output. thanks.



pi@raspberrypi:~/GrovePi/Software/Python/grove_i2c_sunlight_sensor $ python simpletest.py

Press Cntrl + Z to stop



Vis: 263

IR: 297

UV Index: 0.03



Vis: 263

IR: 297

UV Index: 0.03



Vis: 263

IR: 297

UV Index: 0.03



Bill