I have add 4 files in my project:
- pm_static_xiao_nrf54l15_nrf54l15_cpuapp.yml
- sysbuild/mcuboot/boards/xiao_nrf54l15_nrf54l15_cpuapp.conf
- sysbuild/mcuboot/boards/xiao_nrf54l15_nrf54l15_cpuapp.overlay
- boards/xiao_nrf54l15_nrf54l15_cpuapp.overlay
So now I have an issue with TEMP_NRF5_MPSL.
Do you know why?
* Executing task: nRF Connect: Generate config xiao_nrf54l15/nrf54l15/cpuapp for /home/ludovic/matter_light_bulb
Building matter_light_bulb
west build --build-dir /home/ludovic/matter_light_bulb/build_1 /home/ludovic/matter_light_bulb --pristine --board xiao_nrf54l15/nrf54l15/cpuapp -- -DCONF_FILE="prj.conf" -DBOARD_ROOT="/home/ludovic/platform-seeedboards/zephyr"
-- west build: generating a build system
Loading Zephyr module(s) (Zephyr base): sysbuild_default
-- Found Python3: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/local/bin/python3.12 (found suitable version "3.12.4", minimum required is "3.10") found components: Interpreter
-- Cache files will be written to: /home/ludovic/.cache/zephyr
-- Found west (found suitable version "1.4.0", minimum required is "0.14.0")
-- Board: xiao_nrf54l15, qualifiers: nrf54l15/cpuapp
Parsing /home/ludovic/matter_light_bulb/Kconfig.sysbuild
Loaded configuration '/home/ludovic/matter_light_bulb/build_1/_sysbuild/empty.conf'
Merged configuration '/home/ludovic/matter_light_bulb/sysbuild.conf'
Configuration saved to '/home/ludovic/matter_light_bulb/build_1/zephyr/.config'
Kconfig header saved to '/home/ludovic/matter_light_bulb/build_1/_sysbuild/autoconf.h'
--
*****************************
* Running CMake for mcuboot *
*****************************
Loading Zephyr default modules (Zephyr base).
-- Application: /home/ludovic/ncs/v3.1.0/bootloader/mcuboot/boot/zephyr
-- CMake version: 3.21.0
-- Found Python3: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/local/bin/python (found suitable version "3.12.4", minimum required is "3.10") found components: Interpreter
-- Cache files will be written to: /home/ludovic/.cache/zephyr
-- Zephyr version: 4.1.99 (/home/ludovic/ncs/v3.1.0/zephyr)
-- Found west (found suitable version "1.4.0", minimum required is "0.14.0")
-- Board: xiao_nrf54l15, qualifiers: nrf54l15/cpuapp
-- Found host-tools: zephyr 0.17.0 (/home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk)
-- Found toolchain: zephyr 0.17.0 (/home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk)
-- Found Dtc: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/bin/dtc (found suitable version "1.5.0", minimum required is "1.4.6")
-- Found BOARD.dts: /home/ludovic/platform-seeedboards/zephyr/boards/arm/xiao_nrf54l15/xiao_nrf54l15_nrf54l15_cpuapp.dts
-- Found devicetree overlay: /home/ludovic/matter_light_bulb/sysbuild/mcuboot/app.overlay
-- Generated zephyr.dts: /home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/zephyr.dts
-- Generated pickled edt: /home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/edt.pickle
-- Generated devicetree_generated.h: /home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/include/generated/zephyr/devicetree_generated.h
warning: REGULATOR_FIXED_INIT_PRIORITY (defined at drivers/regulator/Kconfig.fixed:14) was assigned
the value '45' but got the value ''. Check these unsatisfied dependencies: REGULATOR_FIXED (=n). See
http://docs.zephyrproject.org/latest/kconfig.html#CONFIG_REGULATOR_FIXED_INIT_PRIORITY and/or look
up REGULATOR_FIXED_INIT_PRIORITY in the menuconfig/guiconfig interface. The Application Development
Primer, Setting Configuration Values, and Kconfig - Tips and Best Practices sections of the manual
might be helpful too.
Parsing /home/ludovic/ncs/v3.1.0/bootloader/mcuboot/boot/zephyr/Kconfig
Loaded configuration '/home/ludovic/platform-seeedboards/zephyr/boards/arm/xiao_nrf54l15/xiao_nrf54l15_nrf54l15_cpuapp_defconfig'
Merged configuration '/home/ludovic/matter_light_bulb/sysbuild/mcuboot/prj.conf'
Merged configuration '/home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/.config.sysbuild'
Configuration saved to '/home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/.config'
Kconfig header saved to '/home/ludovic/matter_light_bulb/build_1/mcuboot/zephyr/include/generated/zephyr/autoconf.h'
-- Found GnuLd: /home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk/arm-zephyr-eabi/arm-zephyr-eabi/bin/ld.bfd (found version "2.38")
-- The C compiler identification is GNU 12.2.0
-- The CXX compiler identification is GNU 12.2.0
-- The ASM compiler identification is GNU
-- Found assembler: /home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk/arm-zephyr-eabi/bin/arm-zephyr-eabi-gcc
=========== Generating psa_crypto_config ===============
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_SPM: False
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_C: True
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER: False
Backup: CONFIG_MBEDTLS_PLATFORM_SETUP_TEARDOWN_ALT: False
Backup: CONFIG_MBEDTLS_THREADING_C: False
Backup: CONFIG_MBEDTLS_THREADING_ALT: False
=========== Checkpoint: backup ===============
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_SPM: False
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_C: True
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER: False
Restore: CONFIG_MBEDTLS_PLATFORM_SETUP_TEARDOWN_ALT: False
Restore: CONFIG_MBEDTLS_THREADING_C: False
Restore: CONFIG_MBEDTLS_THREADING_ALT: False
=========== End psa_crypto_config ===============
=========== Generating psa_crypto_library_config ===============
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_C: True
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER: False
Backup: CONFIG_MBEDTLS_PSA_CRYPTO_SPM: False
Backup: CONFIG_MBEDTLS_USE_PSA_CRYPTO: True
Backup: CONFIG_MBEDTLS_PLATFORM_PRINTF_ALT: False
Backup: CONFIG_MBEDTLS_THREADING_C: False
Backup: CONFIG_MBEDTLS_THREADING_ALT: False
=========== Checkpoint: backup ===============
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_C: True
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER: False
Restore: CONFIG_MBEDTLS_PSA_CRYPTO_SPM: False
Restore: CONFIG_MBEDTLS_USE_PSA_CRYPTO: True
Restore: CONFIG_MBEDTLS_PLATFORM_PRINTF_ALT: False
Restore: CONFIG_MBEDTLS_THREADING_C: False
Restore: CONFIG_MBEDTLS_THREADING_ALT: False
=========== End psa_crypto_library_config ===============
-- Using ccache: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/bin/ccache
-- Found gen_kobject_list: /home/ludovic/ncs/v3.1.0/zephyr/scripts/build/gen_kobject_list.py
MCUBoot bootloader key file: /home/ludovic/ncs/v3.1.0/bootloader/mcuboot/root-ed25519.pem
CMake Warning at CMakeLists.txt:412 (message):
WARNING: Using default MCUboot signing key file, this file is for debug use
only and is not secure!
-- Configuring done
-- Generating done
-- Build files have been written to: /home/ludovic/matter_light_bulb/build_1/mcuboot
--
***************************************
* Running CMake for matter_light_bulb *
***************************************
Loading Zephyr default modules (Zephyr base).
-- Application: /home/ludovic/matter_light_bulb
-- CMake version: 3.21.0
-- Found Python3: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/local/bin/python (found suitable version "3.12.4", minimum required is "3.10") found components: Interpreter
-- Cache files will be written to: /home/ludovic/.cache/zephyr
-- Zephyr version: 4.1.99 (/home/ludovic/ncs/v3.1.0/zephyr)
-- Found west (found suitable version "1.4.0", minimum required is "0.14.0")
-- Board: xiao_nrf54l15, qualifiers: nrf54l15/cpuapp
-- Found host-tools: zephyr 0.17.0 (/home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk)
-- Found toolchain: zephyr 0.17.0 (/home/ludovic/ncs/toolchains/c5be9c56c7/opt/zephyr-sdk)
-- Found Dtc: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/bin/dtc (found suitable version "1.5.0", minimum required is "1.4.6")
-- Found BOARD.dts: /home/ludovic/platform-seeedboards/zephyr/boards/arm/xiao_nrf54l15/xiao_nrf54l15_nrf54l15_cpuapp.dts
-- Found devicetree overlay: /home/ludovic/matter_light_bulb/boards/xiao_nrf54l15_nrf54l15_cpuapp.overlay
-- Generated zephyr.dts: /home/ludovic/matter_light_bulb/build_1/matter_light_bulb/zephyr/zephyr.dts
-- Generated pickled edt: /home/ludovic/matter_light_bulb/build_1/matter_light_bulb/zephyr/edt.pickle
-- Generated devicetree_generated.h: /home/ludovic/matter_light_bulb/build_1/matter_light_bulb/zephyr/include/generated/zephyr/devicetree_generated.h
warning: Deprecated symbol BT_CTLR is enabled.
warning: TEMP_NRF5_MPSL (defined at /home/ludovic/ncs/v3.1.0/nrf/drivers/mpsl/temp_nrf5/Kconfig:8) has direct dependencies DT_HAS_NORDIC_NRF_TEMP_ENABLED && HAS_HW_NRF_TEMP && MPSL && SENSOR && !MPSL_FEM_ONLY with value n, but is currently being y-selected by the following symbols:
- NRF_802154_SL (defined at /home/ludovic/ncs/v3.1.0/nrfxlib/nrf_802154/zephyr/Kconfig.nrfxlib:47), with value y, direct dependencies !NRF_802154_SOURCE_HAL_NORDIC && <choice NRF_802154_SL_TYPE> (value: y), and select condition NRF_802154_TEMPERATURE_UPDATE && !NRF_802154_SOURCE_HAL_NORDIC && <choice NRF_802154_SL_TYPE> (value: y)
Parsing /home/ludovic/matter_light_bulb/Kconfig
Loaded configuration '/home/ludovic/platform-seeedboards/zephyr/boards/arm/xiao_nrf54l15/xiao_nrf54l15_nrf54l15_cpuapp_defconfig'
Merged configuration '/home/ludovic/matter_light_bulb/prj.conf'
Merged configuration '/home/ludovic/matter_light_bulb/build_1/matter_light_bulb/zephyr/.config.sysbuild'
error: Aborting due to Kconfig warnings
CMake Error at /home/ludovic/ncs/v3.1.0/zephyr/cmake/modules/kconfig.cmake:377 (message):
command failed with return code: 1
Call Stack (most recent call first):
/home/ludovic/ncs/v3.1.0/nrf/cmake/modules/kconfig.cmake:83 (include)
/home/ludovic/ncs/v3.1.0/zephyr/cmake/modules/zephyr_default.cmake:131 (include)
/home/ludovic/ncs/v3.1.0/zephyr/share/zephyr-package/cmake/ZephyrConfig.cmake:66 (include)
/home/ludovic/ncs/v3.1.0/zephyr/share/zephyr-package/cmake/ZephyrConfig.cmake:92 (include_boilerplate)
CMakeLists.txt:9 (find_package)
-- Configuring incomplete, errors occurred!
CMake Error at cmake/modules/sysbuild_extensions.cmake:530 (message):
CMake configure failed for Zephyr project: matter_light_bulb
Location: /home/ludovic/matter_light_bulb
Call Stack (most recent call first):
cmake/modules/sysbuild_images.cmake:43 (ExternalZephyrProject_Cmake)
cmake/modules/sysbuild_default.cmake:21 (include)
/home/ludovic/ncs/v3.1.0/zephyr/share/zephyr-package/cmake/ZephyrConfig.cmake:75 (include)
/home/ludovic/ncs/v3.1.0/zephyr/share/zephyr-package/cmake/ZephyrConfig.cmake:92 (include_boilerplate)
/home/ludovic/ncs/v3.1.0/zephyr/share/sysbuild-package/cmake/SysbuildConfig.cmake:8 (include)
template/CMakeLists.txt:10 (find_package)
-- Configuring incomplete, errors occurred!
See also "/home/ludovic/matter_light_bulb/build_1/CMakeFiles/CMakeOutput.log".
FATAL ERROR: command exited with status 1: /home/ludovic/ncs/toolchains/c5be9c56c7/usr/local/bin/cmake -DWEST_PYTHON=/home/ludovic/ncs/toolchains/c5be9c56c7/usr/local/bin/python3.12 -B/home/ludovic/matter_light_bulb/build_1 -GNinja -DBOARD=xiao_nrf54l15/nrf54l15/cpuapp -DCONF_FILE=prj.conf -DBOARD_ROOT=/home/ludovic/platform-seeedboards/zephyr -S/home/ludovic/ncs/v3.1.0/zephyr/share/sysbuild -DAPP_DIR:PATH=/home/ludovic/matter_light_bulb
* The terminal process terminated with exit code: 1.
* Terminal will be reused by tasks, press any key to close it.
Regards