DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

[code]v1.20

  • Improvements in the FFT (Marco Sinatti):
    • The FFT function and FFT source can be selected from the track4 menù, it’s possible to select the ch A or ch B.
      They are displayed as track4 math results.
    • Changed some colors
    • Changed the FFT meter positions, the max meter moves along the peak position
  • Trigger fixes (JackTheVendicator)
  • Fixed volume control + selection bounce (Jerson)[/code]

Thanks everybody



Latest download: https://github.com/pmos69/dso203_gcc/zipball/master