Thanks Marco. Glad you could check it out. ![]()
I noticed the trigger level display bug. Will have to check it…
The frequency scale on the FFT is actually dependent on the x scale sample time.
It’s something like:
Nyquist_freq should be = (1.000.000.000.000 / _T_Scale) / 2
(_T_Scale is in nS)
The whole FFT graph (256 lines) x_scale should cover from 0 to the Nyquist_freq.
so each line in the FFT should be = Nyquist_freq / 256
… I have a build with that value and the top frequency from the FFT displayed.
I’ll just fix the trigger level thing and release it…
here’s the code for those calculations:
[code]
NFreq = (1000000000 / (_T_Scale)) / 2;
NFreq *= 1000;
Int2Str(NumStr, NFreq, F_UNIT, 4, UNSIGN);
Print_Str( 248, 0, 0x0005, PRN, NumStr);
PeakFreq = 0;
imax = 0;
for (i=0; i < (256); i++) {
if (PeakFreq < arrout[i]) {
PeakFreq= arrout[i] ;
imax = i;
}
}
Int2Str(NumStr, ((NFreq / 256) * imax), F_UNIT, 4, UNSIGN);
Print_Str( 92, 0, 0x0005, PRN, NumStr);<e>[/code]</e></CODE></r>