@muslimens
- Yes. The rest is for advanced use. (to program additional features to WC e.g.)
2.) estimate:
[list]
[*] 95%: no changes => the old firmware works
[*] 4%: same problem as me => try another way to reconfigure (see man y examples here in this thread)
[*] 0.9%: get some help to reconfigure
[*] 0.09%: get some special help to reconfigure
[*] 0.01%: bricked[/list]