DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

Did I really miss the point so much? As far as I understood, compatibility with PAWN is a basic feature of the 4 slot version which is in fact a 5 slot version, at least to my understanding of Wildcat’s explanations in this thread. Would it really be such hard work to also feature this in the 3 slot version for slot 2 which is included in the W4.4 archive anyway? (I don’t need the high performance W4.4, as I mainly use the DSO203 to track down problems with model flight hardware)

This point is clear to me, undoubtedly making a complex thing intuitive is quite a challenge. I am not so much into oscilloscopes (DSO203 is my first and currently only one), but I am part of the linux world since 1993, there it’s quite the same. First linux versions were nearly unusable for standard folks, this has changed later.

This would be an option. Another option (about which I currently don’t know if it is an option at all) would be to enhance the UI in a way that some functions are not included by default, but provided as a plugin stored in binary form on the DSO’s “internal USB drive”. Would be a great thing, as codebase would decrease and the present issues with flashing to different hardware probably wouldn’t exist anymore. I am thinking about learning myself to program DSO203 in order to include some of Wildcat’s enhancements into the newer GUI. I’ve already played with the PAWN toolchain (that’s why I want to keep PAWN), but that’s really not the same as programming in C.



Did I get you right - you have been programming UIs for Apollo? I am not familiar to space flight, but that would really have been a great task…