Hello bobtidey
thanks for ur explanations!!
Thats are good news for me, particularly the things with the Slots…ok, i will remember later. I found the original SYS and APP from my Devices. But also a newer one, SYS V1.61 and APP V1.11. Its this also OK ? u know it what its better as the SYS V1.160 an APP V1.10 ?
When i change the sys or/and APP, must i calibrate the device again, or one time its enough??
a other question: i found : PA1_110. PA3_110 and PA1_111, PA3_111 and …FPGA´s and also AP1_100… whats this? How i can use this Files?
I think for the beginning its better, i load all Files for Trying in Slot 3+4. Then i can tryit and the original Firmware its not broken. Later i can also load the system what i want to use in Slot 1+2…right!? The firmware from wildcat33, must i load all 3 files or only one?
Ok, i think i have enough Information for trying. Thank u!!
Greetings…klaus